Wiser

The Smart Heating Control System

We provide beautifully simple smart heating control systems that make it easy for you to control the heating in your home.

Room-by-room scheduling
30 day money back guarantee
3 year warranty
Easy installation
Money saving features
Award winning

How Wiser works

 

Wiser is made up of Room Thermostat, Radiator Thermostat, and the Wiser Plug. These are all linked by the brains of the operation – the Heat HubR and controlled via the Wiser Home App. You only need one Heat HubR per system and you get one in every Thermostat or Multiroom Kit.

You can build your system as you go using Wiser Radiator Thermostats and tailor it to your personal needs. Scroll down to find out how you can make significant energy savings with Wiser.

Smart heating controls by Wiser could reduce
your annual energy bills by up to 30%

Wiser takes care of the heating bill,
so you can take care of more important things

Did you know, over 50% of a home’s energy consumption is used for heating and hot water? 

So when it comes to heating your home it’s time to get Wiser.

 

Smart thermostat system percentage savings based on BEAMA and Salford university research statistics 2021. Energy mode savings based on Schneider Electric research on Wiser user data 2021.

Savings are guideline and will vary based on your home's thermal performance.  
  

Wiser control

Research shows that upgrading to a smart programmable thermostat like Wiser from basic Class I heating controls could save up to 18% energy usage (BEAMA 2021)

Wiser modes

Superior energy-saving features like Away Mode, Eco Mode and weather compensation have been shown to save up to 16% on energy bills.

 

Wiser rooms

Upgrading from basic to smart controls plus the addition of room-to-room control, like smart radiator thermostats, can save over 30%* on heating and hot water bills.

 

*% saving based on upgrading from basic Class I heating controls to a smart multi-room

programmable thermostat system from Wiser and correctly utilising Away Mode and Eco Mode

More about smart modes

Activate the following smart modes to maximise comfort and efficiency.

 

  • Smart Modes – Can reduce energy usage by up to 16%. By lowering the temperature when you’re away from home with Away Mode you can reduce your bill by 14%. Eco Mode can reduce your energy usage by another 2% by finding the most economical way to run your smart heating system.
  • Comfort Mode – ensures your heating reaches the set temperature at the right time maximising comfort throughout your home.
  • Geofencing via IFTTT - enables Wiser to automatically activate Away Mode when you leave the home.

"OK Google, turn off the heating in the bedroom"

Use the Google assistant? No worries, Google Home can adjust your thermostat and let you make changes using voice commands too. After setting up the Wiser smart heating system, go to the Google Home app and select Home Control from the Assistant menu. Tap '+' and search Wiser Heat, enter your Wiser log-in to connect your account, assign your Wiser devices to your rooms and you're done! OK Google, turn on the hot water at 6am”

 

   

 

"Alexa, turn on the heating."

Wiser is of course Alexa compatible. After setting up the Wiser smart heating system, go to the Alexa app and select Skills & Games. Search Wiser Heat and select Enable Skill, enter your Wiser log-in to connect your account, and you're done! “Alexa, turn on the heating at 5pm”

 

    

 

IFTTT compatible

IFTTT allows you to create personalised commands based on 'triggers' and 'actions' within minutes.
Link Wiser to your IFTTT account and download applets to turn Away Mode ON when you leave the house, and OFF on your return.
Once Away Mode is ON, Wiser automatically reduces all set-points to the Away Mode levels you've chosen in the Settings menu. By turning the heating down automatically, it saves you energy and money without needing to interact with the app.
 

Wiser Home App

Room-by-room heating

Whether you’re a sofa lounger, an exerciser or a bit of an all-rounder, multi-room heating controls mean everyone can get the temperature just how they like it… in every room.

 

Insights and heat report

A Wiser home is a more environmentally friendly home. Save energy, and money by learning more about your home heating with insights

Boost! Feeling a little chilly? You can boost temperatures and override your heating schedule for a short period to keep cosy. Boost individual rooms or the whole house.

 

Simple Schedule changes

Whether you’re an on-the-goer or an afternoon napper you can schedule your heating to suit your lifestyle. And if your routine changes your heating can change with a tap of the app.

"We've been impressed with it...The Wiser heating system does exactly what it promises: it’s easy to install and easy to use."

-Tech Advisor

“I set Wiser up with IFTTT as well so I can have the system go into 'Away Mode' when me and my wife leave the house." 

-Trust Pilot

-"Simplicity is the name of the game ... If you want multi-room heating on a reasonable budget, there’s nothing that comes close."

-Trusted Reviews