Portable Power

Designed for outdoor enthusiasts and home users to provide consistent, reliable power whenever you need it - anytime, anywhere.


Loading Products...

What is a portable power station?

A portable power station is like a big, rechargeable battery that you can take anywhere. It's handy for camping, outdoor events, or as a backup power source at home. You can plug in various devices like phones, laptops, and even small appliances to keep them running when there's no traditional power source available. It's also cleaner, quieter and safer than a traditional fuel-based generator

Discover the Schneider OffGrid Portable Power Station

Reliable

Whether you're at home or on the road, OffGrid delivers up to 700W of power in a device that is an average of 20% lighter than the competition.

Adaptable

OffGrid can charge up to 11 different devices and can recharge with a standard AC plug, solar, car, and USB-C.

Sustainable

With 60% post-consumer recycled plastic casing, energy-saving mode, and optional solar panels, OffGrid is a leading sustainable portable power station.

Features of the OffGrid Portable Power Station

  1. Up to 700W of power and an average 20% lighter
  2. Casing made from 60% post-consumer recycled durable material
  3. Wireless charging pad
  4. Multiple AC and USB outlets
  5. Advanced LCD display
  6. Four ways to recharge

Emergency LED Light

Ambient LED light panel with SOS lighting mode allows for easy usage even in darker settings, such as a camp site at night or during a power outage.

Say goodbye to downtime

Did you know that solar energy is one of the most popular and sustainable methods of recharging? All our OffGrid Portable Power Stations are compatible with a dedicated solar panel accessory designed to provide you with continuous, renewable power no matter where you go.

FAQs

What is a portable power station?

What are the benefits of OffGrid Portable Power Station?

How long will a OffGrid Portable Power Station run?

How do you charge the OffGrid Portable Power Station?

What factors should I consider when buying a portable power station?

Is it safe to leave my OffGrid Portable Power Station plugged in all the time?