Energy Monitoring

from $376
<p>Energy Monitoring</p>

Schneider Energy Monitor

Formerly known as Wiser Energy Home Power Monitor, it helps you manage the electricity usage in your home, from the circuit to the plug level using the Schneider Home app. The app provides meaningful insights for you to take control of your energy usage and find ways to reduce your electric bill.

Take control to lower your electricity bills.

  • Save Energy. Save Money. See and manage how much energy your home is consuming and uncover what it’s costing you.
  • Get real-time notifications. Keep your home running smoothly. Compressor not running often enough? Reached a peak energy usage when you shouldn't have? Set custom notifications to stay in-the-know.
  • Monitor your home from anywhere. Know what's happening at any time. No matter where you are, the Schneider Home app will keep you informed on what’s happening in your home.
  • Gain more control. Manage at the circuit, plug and switch level. Get more insight and control over your energy use with Square D Control Relays and Schneider X series connected wiring devices.
  • Have solar? Maximize your solar energy use. Compare solar production and energy consumption side-by-side in a single view so you can maximize the power you make and minimize the power you buy.

  • Installs in most 120/240V panels up to 200A by a licensed electrician in less than 30 minutes.


    The Schneider Energy Monitor is available with either one or two pairs of current transformers (CTs). While most homes will need just one set, you should opt for two if you have solar panels, a dedicated circuit, a whole-home backup generator, or 400A split-service.

    Schneider Energy Monitor

    With 1 pair of CTs

    With 2 pairs of CTs

    Real-time Energy Monitoring
    Yes
    Yes
    Custom notifications
    Yes
    Yes
    24/7 Visibility
    Yes
    Yes
    Monitors your home's solar panels
    No
    Yes
    Monitors a dedicated circuit, whole-home generator or 400A split-service
    No
    Yes

    Schneider Energy Monitor

    With 1 pair of CTs
    With 2 pairs of CTs
    Real-time Energy Monitoring
    Custom notifications
    24/7 Visibility
    Monitors your home's solar panels
    Monitors a dedicated circuit, whole-home generator or 400A split-service
    Wizeremz
    Schneider Energy Monitor ​(1 set of CTs)
    Monitors the main energy in your home.
    Wiserempvz
    Schneider Energy Monitor ​(2 set of CTs)
    Monitors the main energy in your home plus one of the following: solar, dedicated circuit, whole-home generator, 400 A split-service.

    FAQs

    Is a Schneider Energy Monitor compatible with my home?

    Do I need Wi-Fi to use the Schneider Energy Monitor?

    Will the Schneider Energy Monitor work with my solar panels?

    Is there a subscription fee?

    Hear it from our Customers

    1
    George B

    The monitor has been a game-changer. It's helped me become more aware of which devices are using the most electricity, enabling me to make smarter decisions about when and how to use them. Already, I've noticed a positive impact on my utility bills by reducing usage during peak hours.

    2
    Brandon

    It has saved me so much money by helping me know what was driving up my electric bill.

    3
    Ryan F

    I can say without hesitation that this product paid for itself quite easily within just a few days of installation. I'm a solar power generator, so that makes the product even more useful for me.