Introducing the all new Square D™ switches, dimmers, sensors and outlets with a one-of-a-kind interchangeable design with flush screwless wall plates
Same device, two distinct looks
Easily update the look of your devices without rewiring with Square D’s unique interchangeable wall plates.


Switches, sensors and smart outlets
✓ Flexible and feature-rich
These switches, sensors, dimmers and outlets set the new benchmark for how today's wiring devices should look and feel.
✓ Fast USB charging
You can even charge two devices at once using our faster-than-average outlets with high-amperage USB charging.
✓ Monitor your energy use
With smart outlets and switches you can monitor energy usage and control lighting through our suite of smart home apps. Assistant-enabled devices.
Connected Home Product of the Year
By adding energy monitoring at the switch and plug level, homeowners can make smarter decisions about energy use, costs and carbon footprint. Square D X and XD Series Connected Wiring Devices have been recognized by IoT Breakthrough Awards as the Connected Home Product of the Year!


X Series available now
As the best value in wiring devices, X Series is surprisingly feature-rich, including easy installation, refreshed modern design, and smart home compatibility.


Simple control with the Wiser Home app
✓ Remote control
Turn lights and appliances on or off from your mobile phone
✓ Automate lighting
Set up schedules to turn lights on or off based on sunrise/sunset
✓ Works with Alexa and other home assistants
Expand automation through your popular home assistants
✓ Energy monitoring
See how much energy each connected device uses
Wiser™ Home app
How it works
The Wiser™ Home app from Schneider Electric gives you the ability to see how much energy you're using, control devices remotely, set automated schedules, and so much more. You can get even more advanced energy insights when you add the Wiser™ Energy home monitor.


“This was a really easy switch to install. Would definitely recommend. I am not an electrician but this was understandable for someone who does small projects in their home.”
Michellerem from Scranton, PA


“This switch outlet is a nice addition to my smart home. It was super easy to install. It only took about 10 min to install it and get it connected to the app. It even connects to our Alexa device so we can turn the lamps on with just saying turn the light on. Would definitely recommend!”
Kevisfxstb from Florida


Use your phone to control connected outlets and light switches
✓ Smart outlets and grid-to-plug intelligence
You can now monitor energy usage and control lighting through our suite of smart home apps.
✓ Connectivity
Equipped with WiFi, these outlets and switches also pair with Alexa and other voice-activated devices.
Faster installation, more safety:
Richer features for homeowners and electricians alike
1. Black tamper-resistant shutters
Put safety at the forefront without making it obvious, with easy-sliding shutters.
2. Ground wire hole
Install faster utilizing this innovation for quickly wrapping the ground wire to the ground screw.
3. Side-mount pressure plates
Speed wiring time with better accessibility.
4. Bigger cutout for wider snips
Enjoy the ease of an easy-access cutout space for speedy wire snips.
5. Self-grounding clip
Skip the separate ground screw.
6. Wire push-in
Connect your wire quickly with push-in option and avoid the need to wrap.