Wiser Energy, Home Energy Monitor, Wifi, with 1 pair of CTs
- Keep tabs on your home activity from anywhere
- Easy installation in your home's electrical panel
- Reduce your electric bill with live energy tracking
- Integrates with Alexa, Google, Square D connected Wiring devices and more
WISEREM: For homes without a solar power system
If you have a standard residential home without a solar power system, you'll want the standard Wiser bundle, WISEREM, that includes one pair of current transformers to monitor energy use.
You may want to add a second set of current transformers if any of these apply:
1. Support for 400A split-service panels; or
2. Ability to monitor up to two 120V or 240V dedicated circuits in order to track a major appliance or device; or
3. Tracking for home standby generators.
WISEREMPV: For homes with a solar power system
If your home has a solar power system, you'll want the Wiser bundle, WISEREMPV, that includes a second pair of current transformers to monitor energy use and solar production.
You'll get the Wiser Energy monitor, plus a second set of current transformers to measure solar production.




Real-time energy monitoring to save you money
The Wiser Energy system installs in your home's electrical panel and provides real-time energy usage, notifications when devices turn on or off, and can help you save money and avoid disaster. Using the Square D™ version of the Sense app, keep tabs on your home anywhere, from your phone.


How Wiser gets smarter over time with machine learning
✓ Wiser Energy Home Power Monitor gradually learns about your home as things turn on and off.
✓ Wattage is tracked through current transformers wrapped around the mains that feed your elecrical panel, sampling data 1 million times per second.
✓ Machine learning algorithms find device signatures within your home's power profile and uses that data to determine what devices are on and off.
✓ Typically the monitor detects 12 devices in the first month after it’s installed and 25-30 devices after 12 months.
Installation
Installing the Wiser Energy system is simple, quick and straightforward.* Once the Wiser Energy monitoring unit is installed in your home's electrical panel by a licensed electrician, and connected to your wifi, setting up the app takes only minutes.
Once your devices are identified, you'll have crystal clear insight into your energy use. Now your home has a voice!
*Note: Contact a licensed electrician for installation of the Wiser Energy system.
What’s in the box:
Monitor
Mounting Bracket (optional) with 2 Screws
Antenna Assembly
Power Cable
1 Pair of Current Transformers
Manual
* 2-pole breaker not included


range of product |
Wiser |
---|---|
Product or Component Type |
Monitoring unit |
Height |
2.6 in (66.04 mm) |
Width |
5.4 in (137.16 mm) |
Depth |
1.3 in (33.02 mm) |
IP degree of protection |
IPx0 |
Category |
00105-WISER ENERGY PRODUCTS |
Discount Schedule |
DE3A |
GTIN |
785901218104 |
Nbr. of units in pkg. |
1 |
-
How does Wiser Energy work?
With just two clamp-on current sensors, the Wiser Energy Monitor takes current and voltage measurements over 1 million times every second.
From this incredibly high-resolution data, it derives the electrical signatures of individual devices. In comparison, most "high resolution" smart meters only take measurements every couple of seconds... hardly real time!
Within the first week of installation, Wiser Energy should be able to find some common devices that cycle on and off frequently, like your refrigerator or microwave. Some devices will take longer to identify, until the algorithms have seen enough contextual data to reliably detect them.
There are devices that Wiser Energy won't be able to recognize right away, but as more Wiser Energy Monitors are installed across the US and Canada, the machine learning algorithms will have more data to generate models from, and the device detection capabilities will just keep growing!
-
Is Wiser Energy compatible with my home?
To ensure you have the best experience with Wiser Energy, the following compatibility specifications are recommended:
Your home has:
- A consistent 2.4Ghz Wi-Fi connection. Wiser Energy is not compatible with 5Ghz Wi-Fi signals.
- Its own electrical meter and accessible electrical panel.
Your mobile device runs on iOS or Android and has Bluetooth and Wi-Fi connectivity.
Your electrical panel:
- Is a split-phase 120/240V residential panel up to 200A.
- Must have enough space to fit sensor clamps with HxWxD dimensions of 3.375" x 2" x .75" (85.73 x 50.8 x 19.05mm), and an inside diameter of 1”. The Wiser Energy current sensors may not be able to fit around busbars.
- Should be within cable length of Sensor cables (46" (116.84cm) and power cable (36" (91.44cm) ).
- Does not drop below 32°F (0°C) or exceed 122°F (50°C). Is not exposed to water or areas with high condensation (Sense complies with ANSI/IEC 60529 Rated IPx0).
The following Square D electrical panels are known to be incompatible as a result of the current sensors not fitting around the bus bars:
QC12L200C QC2442M200C QC816F125C QC816F150C QC816F200C RC12L200C RC1624M100S RC1624M125S RC2040M125CH RC2040M150CH RC2040M200C RC2040M200CH RC816D200CH RC816F100CH RC816F125CH RC816150CH RC816F200C RC816F200CH SC1624M100F SC1624M100S SC1624M125F SC1624M125S SC2040M125F SC2040M125S SC2040M200F SC3040M200F SC3040M225F SC816D150C SC816D200C SC816D200F SC8L125F SU2040M200C SU3040M200R SU2040M225R SU816D150C SU816D200C SC2040M200C SO2040M200S -
Will Wiser Energy work with my solar panels?
Most likely! Your incoming solar feed can connect directly into your main electrical panel, either through a breaker or a service-side tap.
If solar is set up in a subpanel, the incoming solar feed should be within 46" of the main panel as this will allow the provided current sensor cables to reach and connect to the Wiser Energy monitor in the main electrical panel.
If it is further than 46", extension cables are available in lengths of:
Length (Feet) Part Number 4 WISEREMCTEXT4 12 WISEREMCTEXT12 25 WISEREMCTEXT25 40 WISEREMCTEXT40 These extensions can be combined to achieve larger lengths, but the maximum length can be no more than 300'.
-
Can Wiser Energy detect all devices?
Not everything. We're able to identify many electrical devices in typical homes and continue to expand our device detection abilities. As we examine data from more homes, the performance and coverage of our device detection will improve.
-
How does Wiser Energy keep my data secure?
We take security very seriously and we do everything we can to ensure data is secure. All communications between the Wiser Energy monitor, the cloud servers, and Wiser Energy apps are encrypted with AES 128-bit encryption and TLS/SSL (HTTPS).
Wiser Energy uses Amazon Web Services (AWS) for cloud servers and online storage. Personally identifiable information like email address and account information is stored in physically separate systems from any application data.
Physical security is managed by Amazon and access to these production systems is limited to a very small group of engineering team members.
Automated systems process the data collected from Wiser Energy monitors to detect devices, send notifications, generate report emails, and power the Wiser Energy apps.
This data is never shared with 3rd parties without explicit user opt-in on a case-by-case basis (for example, when a utility wishes to provide discounts/services to their customers in exchange for sharing limited power data.)
Support employees will on occasion need to access some of this data to troubleshoot issues, but we will only access this data with explicit permission.