Switches, Sensors and Outlets

Modern design and functionality in switches, dimmers, room sensors and outlets

Schneider switches, dimmers, sensors and outlets with a one-of-a-kind interchangeable design with flush screwless wall plates

Loading Products...

Feel the good energy throughout your home with Schneider.


Remote monitoring and control

With connected outlets and switches, control lighting, appliances and more with the Schneider Home app or voice-activated assistants.

Flexible and feature-rich

These switches, sensors, dimmers and outlets set the new benchmark for how today's wiring devices should look and feel.

Fast USB charging

Charge two devices at once using our faster-than-average outlets with high-amperage USB charging.

What is Matter?

With so many different connected devices out there, it can be cumbersome to connect and control them through multiple apps from multiple brands. Matter simplifies that.


Matter is the new communication protocol that allows certified devices from different brands to work together across Matter-compliant platforms with just one app.


Learn more

Connected Home Product of the Year

Video Play Icon

Same device, two distinct looks

Easily update the look of your devices without rewiring with Schneider’s unique interchangeable wall plates.

Simple control with the app

  • Turn lights and appliances on or off from your mobile phone
  • Set up schedules to turn lights on or off
  • See how much energy each connected device uses
  • Expand automation through your popular home assistants

FAQs

What is Matter?

Which smart hubs/controllers support Matter?

What do I need for using a Matter device?

What app do I use with my device?

What is the Matter firmware/software requirements for each platform?

What if I don’t have any of the Matter ecosystems? Can I still use these devices and what app do I use?

What happens if my hub gets disconnected from internet but still has local Wi-Fi connectivity?

Is an internet connection needed for my Matter-compatible Schneider X Series devices to work?

Will my Matter-compatible Schneider X Series products work with Matter devices from other brands?

Are my current Schneider X Series Wi-Fi devices compatible with Matter?

Is there a limit of devices that I can connect to my network?

How safe is Matter from a cybersecurity perspective?

Can I share my device from one ecosystem to the other?

Is Matter similar to Zigbee?

How to reset my Matter-compatible Schneider X Series device?

Do I need a neutral cable for Matter-compatible Schneider X Series device?

Are my Matter devices compatible with my home?

What will happen if a Matter hub/controller is removed from the App?

How to connect the Matter-compatible Schneider X Series matter Devices, if I change my Wi-Fi network name or password or I change my router?

Will Matter-compatible Schneider X Series devices connect to a 5GHz network?

Why does my Matter-compatible Schneider X Series devices show "No Response"?"

What should I do if my Matter-compatible Schneider X Series device is offline?